LTE FDD
For Waveform Playback (ARB) capability.
This button is displayed when a Basic Downlink carrier is selected in the categories of the upper pane.
Click the Test Model button in the Basic Downlink FDD Node to access the Test Models.
|
SCPI Command |
[:SOURce]:RADio:LTEFdd:WAVeform:CCARrier<n>:DLINk:CONFig:TEST <string> |
|
SCPI Example |
:RAD:LTEF:WAV:CCAR:DLIN:CONF:TEST "TestModelType:ETM12,SystemBandwidth:B10M" |
|
Notes |
Sets only (Immediate Action) |
|
Preset |
Refer to the element definition of the data part below. |
|
State Saved |
No |
|
Range |
Refer to the element definition of the data part below. |
|
Initial S/W Revision |
A.20.01 |
|
Settings |
Symbols in the data part |
Values in the data part |
Preset values |
|
Test Model Type |
Test Model Types |
ETM11 | ETM12 | ETM2 | ETM2A | ETM31 | ETM31A | ETM32 | ETM33 | ETM11REP | ETM11REPT |
|
|
System Bandwidth |
System Bandwidth |
B1M4 | B3M | B5M | B10M | B15M | B20M |
B10M |